Product FAQs

Ask a Question

Do the Altivar 61/71 Drives have internal surge supressors?

Issue:
Do the Altivar 61/71 Drives have internal surge supressors?

Product Line:
Altivar 61/71 Drives

Environment:
All products of Altivar 61/71 Drives

Cause:
N/A

Resolution:
Yes but only in the Higher Horsepower Drives. It is included in the EMC filter boards
Was this helpful?
What can we do to improve the information ?