Product FAQs

Ask a Question

Independant HMI screens when we change pages in Vijeo Design Air, Plus or Webgate

Issue:
Independant HMI screens when we change pages in Vijeo Design Air, Plus or Webgate

Product Line:
Vijeo Designer

Resolution:
It is not possible to change pages on Vijeo Design Air without the pages changing on the HMI because Vijeo Design Air is always synchronized with the HMI. 
However, the Web Gate allows you to display the pages of the HMI with or without the synchronization. 
Vijeo Design Air Plus also allows you to build the pages different than the HMI pages. 
Was this helpful?
What can we do to improve the information ?