Product FAQs

Ask a Question

Does SoMachine V4.2 include the ATV process (ATV600 and ATV900) DTMs?

Issue:
Does SoMachine V4.2 include the ATV process (ATV6xx and ATV9xx) DTMs?

Product Line:
SoMachine V4.2

Resolution:
The ATV process DTMs are not yet validated and integrated within SoMachine V4.2. You will have to manually import an EDS file for these drives in order to control them through SoMachine.
They will be in SoMachine V4.3
Was this helpful?
What can we do to improve the information ?