Product FAQs

Ask a Question

What are the part numbers for SoMachine 4.2 software?

The part numbers for SoMachine 4.2 software are:

- SOMNACCZXSPAZZ - SoMachine V4 License Single - Single (1) License with Mandatory registration
- SOMNACCZXTPAZZ - SoMachine V4 License Team - Team (10) License with Mandatory registration
- SOMNACCZXEPAZZ - SoMachine V4 License Entity - Entity (100) License with Mandatory registration

Note: the part numbers for SoMachine 4.3 are the same, the customer will have to specify that he wants version 4.2
Was this helpful?
What can we do to improve the information ?