Product FAQs

Ask a Question

Wha can cause SoMachine V4.1 SP2 to be half online and offline with the controller?

The "All variable" windows when open or minimized as shown below can do that.  It is recommended to close the "All Variables" windows.  Do a clean, build, and download.  In some cases you may need to restart SoMachine.


Was this helpful?
What can we do to improve the information ?