Product FAQs

Ask a Question

Can you have the same password for both Project protection and application protection in Somachine Basic?

Issue:
Can you have the same password for both Project protection and application protection in Somachine Basic?

Product Line:
M221, TM221

Environment:


Cause:


Resolution:
Yes, you can use the same password for both project/application protection.
Was this helpful?
What can we do to improve the information ?