Product FAQs

Ask a Question

Can I update an M241 application with an SD card if the User manager is enabled?

If the user management is enabled, it is not possible to update the application via SD card. The script which is on the SD card is blocked by the user management and will not be executed successful.
 
To update an application with enabled user management it is necessary to connect with SoMachine or at least with the Controller Assistant (manage image to change the application) to the controller.
Was this helpful?
What can we do to improve the information ?