Product FAQs

Ask a Question

What is the maximum number of tasks supported by the LMC058 motion controller?

The maximum number of tasks you can define for the Modicon LMC058 Motion Controller are: 
Total number of tasks = 21 
Cyclic tasks = 4 
Freewheeling tasks = 1 
Event tasks = 8 
External Event tasks = 8 
Was this helpful?
What can we do to improve the information ?