Product FAQs

Ask a Question

M251 boot up time

Issue:
What's the M251 boot up time?

Product Line:
M251

Resolution:
According to the validation lab, it takes around 20-25 seconds for the M251 to start. 
It could take up to 30 seconds with applications where a lot of code is called. 
Was this helpful?
What can we do to improve the information ?