Product FAQs

Ask a Question

Error code 3 on MC_ReadAxisError_ILX function block

Issue:
Getting Error code 3 on MC_ReadAxisError_ILX function block

Product Line:
ILA servo motor

Resolution:

Please use CIA405.GetState function block to check the CANopen state (5=OPERATIONAL) before calling any motion FB. It is possible that there is a call of one or more motion FBs before the CAN initialization is finished. If the error is still present, please check the CANopen settings, wiring and the termination (See attached)
 
Was this helpful?
What can we do to improve the information ?