Product FAQs

Ask a Question

What is the CFi fault on an Altivar Process Drive?

Issue:
What is the CFi fault on an Altivar Process Drive?

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
Principle:
Invalid Configuration Fault (CFi)
If a configuration has been loaded which is inconsistent (invalid parameter value, the functions configured are incompatible, etc.), the drive state changes to CFI fault.
This fault will be reset automatically once a consistent configuration has been loaded or as soon as a correct value is set for the parameters.

Probable cause:
The configuration loaded into the drive via serial link is invalid.

Remedies:
  • Check the loaded configuration.
  • Load a valid configuration.



 
Was this helpful?
What can we do to improve the information ?