Product FAQs

Ask a Question

Side clearance for Blokset

Actually, there is no specific requirement for side clearances. Generally, we recommend same as rear which will be 100 mm. In the case of compensation of energy cubicle (PFC), ventilated, this minimal space will be 200 mm.

It is better to keep 700-800 mm gap from the wall, the criteria is that, some person should be able to walk here and access the screws which are used to mount  the side panel. It is mainly required for easy maintenance. 

But with 100 mm to 200 mm gap, it is manageable but maintenance would be difficult and accessibility would be a problem. So to conclude, we propose  700-800 mm gap in general. But if there is no space available at all, at least 100 - 200 mm gap is mandatory.
Was this helpful?
What can we do to improve the information ?