Product FAQs

Ask a Question

Installed Somachine v4.2 and download to the Magelis. Getting error: "Application has halted. Not enough memory for initialization procedure" when on Web Gate. How to fix the issue?

Issue:
Installed Somachine v4.2 and download to the Magelis.  Getting error: "Application has halted. Not enough memory for initialization procedure" when on Web Gate.  How to fix the issue?

Product Line:
Vijeo Designer, Magelis, Web Gate, Webgate
 
Environment:
 
 
Cause:
 
 
Resolution:
This is a known issue with Vijeo Designer that was installed with Somachine v4.2.  The issue was resolved by installing the latest service pack for Vijeo Designer v6.2 (SP5 or higher).  Redownload the application onto the Magelis.
Was this helpful?
What can we do to improve the information ?