Product FAQs

Ask a Question

What are the system requirements for SoMachine Basic v1.5?

This software can be installed on a personal computer having the following hardware:
  • Processor                            Core 2 duo or better
  • RAM Memory                       2 GBytes or greater
  • Hard Disk                            600 MBytes
  • Display                                1280 x 768 pixels resolution or better
  • Peripherals                           Mouse or compatible pointing device
  • Peripherals                           USB interface
  • Web access                         Web registration requires Internet access
Was this helpful?
What can we do to improve the information ?