Product FAQs

Ask a Question

What are the operating systems supported by SoMachine Basic v1.5?

SoMachine Basic v1.5 is supported on the following operating systems:
  • Microsoft Windows 10 (validation done from V1.4 SP1)
  • Microsoft Windows 8.1 Professional Edition 32 Bit & 64 Bit
  • Microsoft Windows 8 Professional Edition 32 Bit & 64 Bit
  • Microsoft Windows 7 Professional Edition 32 Bit & 64 Bi
SoMachine Basic requires Administrator rights to be installed.
Remove any USB connection to the controller when installing or uninstalling SoMachine Basic.
 
Was this helpful?
What can we do to improve the information ?