Product FAQs

Ask a Question

What is the replacement for Berger Lahr motor with ID number 66307100042 ?

The Berger Lahr integrated motor with ID number 66307100042 is available from Schneider Electric under a new part number.

The original motor with ID number 66307100042 came equipped with a gearbox.

Schneider Electric no longer offers the motor with the gearbox pre-installed so you must order each component separately.

The motor ordering number is ILE1F661PB1A0
The gearbox ordering number is GBX060040K
The adapter kit for mounting the gearbox to the motor is GBK0600660E

Attached to this knowledge article you will find the data sheet for each item.
When all these items are combined they will be the equivalent of 66307100042.


Rev 8-16-18
Was this helpful?
What can we do to improve the information ?