Product FAQs

Ask a Question

Can I increase the number of open windows allowed in Unity Pro beyond 6?

Yes. You can use the following script:
 
  • Unity  Pro limits the number of simultaneous opened editors to 15 for the first session & 6 for subsequent sessions.  This limitation is set by a Windows parameter & can be removed by modifying the registry as indicated below:
  •  From the Registry editor::
            HKEY_LOCAL_MACHINE\System\CurrentControlSet\
           Control\Session Manager\SubSystems
 
-        In the right screen, double click on the ‘Windows’ name to open the string modification window.
-        Find the SharedSection string in the data value. This parameter specifies the system & desktop heaps using the following format:
           SharedSection=xxxx,YYYY,zzzz
           The values are specified in kilobytes.
 
-      The second SharedSection value (YYYY) controls the size of the desktop heap (used for windows objects).
        If on your machine, YYYY is < 8192 then set YYYY to 8192.
 
Under Windows XP & some Windows Vista machine, this value is by default 3072.     System must be restarted.
 
 

R-101317
 
Was this helpful?
What can we do to improve the information ?