Product FAQs

Ask a Question

Is it possible to copy the program out of an LMC20 motion controller?

Yes, it is possible to copy the program out of an LMC20 motion controller.

There can be instances in which an LMC20 needs to be replaced and the program that is stored inside the LMC20 needs to be copied so that it can be loaded into the replacement LMC20.
If you do not have access to the original source code and the programming environment CoDeSys you will therefore need a software tool known as CoDeSys Service tool.
1. In the file selection box of the upload function, type manually "DEFAULT.PRG" (in capital letters !!!) and upload it
2. then, type "DEFAULT.CHK" and upload again.

The saved files can then be downloaded into the replacement LMC20.

With the CoDeSys Service tool, you can upload the boot project from the LMC20 to your PC.
For this, use the function "File -> Upload" in the Service tool.
The boot project contains of 2 files:

Rev 8-1-18




 
Was this helpful?
What can we do to improve the information ?