Product FAQs

Ask a Question

What is the Schneider Electric part number for the 6 pin cable-side motor connector for BRS3 and VRDM3 three phase stepping motors?

The connector that is found on the end of the motor power cable and mates to the motor connector has a part number of 62501504001 and is available as a spare part.

Rev 7.20.17

 
Was this helpful?
What can we do to improve the information ?