Product FAQs

Ask a Question

Error "Number of variables exceeds the maximum allowed. [500]" appears when building Vijeo Designer application

This error occurs when you build an application that has more than 500 variables with the property "Log User Operations on Variable" enabled. To resolve this issue, please limit the application to use 500 or less variables with this property enabled.
Was this helpful?
What can we do to improve the information ?