Product FAQs

Ask a Question

Available Shortcuts within ION Setup

Issue
Looking for a list of available shortcuts within ION Setup v3.0.

Product Line
ION Setup 3.0

Environment
ION Setup

Cause
Completion of tasks and troubleshooting within ION Setup in a more efficent manner.

Resolution

Mouse over select module manager
Show module count and max number of modules allowed.


 
Ctrl+Mouse over selected module manager
Show module manager handle


 
Mouse over selected module
Show module name (as opposed to module label)



Ctrl+Mouse over selected module
Show module handle



Ctrl+Right click on module or module manager
Show menu of applicable ION methods



Shift+Click on module's Output Register
Show output register value. To manually edit the output register value, click on the list item that appears and enter a new value.




Right click > Ctrl+Insert Module
Show menu to select an arbitrary list of modules to be created. Useful when you what to create a module with the highest possible module number.



Ctrl+Upgrade(Assistant)
Upgrade FW only, without pasting a template.



Shift+Upgrade(Assistant)
Upgrade with additional debugging enabled. Not sure what this is, probably additional info on the .log files in the ION Setup folder.



Ctrl+Send(Assistant)
Prompt to disable template checking.

Was this helpful?
What can we do to improve the information ?