Product FAQs

Ask a Question

Is it possible to operate Lexium 32 from DC bus only?

Yes, it is permitted to power and operate Lexium 32 directly from the DC bus only.

See attached presentation.

Note: You will need expert mode access in SoMove to modify the parameter for monitoring of missing mains phase.  The password for expert mode is 696969

Rev 8-21-17
Was this helpful?
What can we do to improve the information ?