Product FAQs

Ask a Question

What is the transient overcurrent rating for the ATV600 and ATV900 series drives?

Issue:
What is the transient overcurrent rating for the ATV600 and ATV900 series drives?

Product Line:
ATV600, ATV900

Environment:
All models, All serial numbers, normal and heavy duty.

Cause:
Information difficult to find in current literature.

Resolution.
The ATV600 series, Normal duty is rated for 110% for 2 seconds and 110% for 60 seconds.
The ATV600 series, Heavy duty is rated for 150% for 2 seconds and 150% for 60 seconds.
The ATV900 series, Normal duty is rated for 120% for 2 seconds and 120% for 60 seconds.
The ATV900 series, Heavy duty is rated for 150% for 2 seconds and 150% for 60 seconds.


 
Was this helpful?
What can we do to improve the information ?