Product FAQs

Ask a Question

Description of P1-46 on LXM28 drive

Issue:
Description of P1-46 on LXM28 drive

Product Line:
LXM28

Resolution:
That parameter is for ESIM output resolution.
Default is 2048 counts from the encoder output based on 1 rotation of the motors encoder at 1280000 counts
Was this helpful?
What can we do to improve the information ?