Product FAQs

Ask a Question

Latest firmware for the TM251MESE using SoMachine V4.3

Issue:
What is the latest firmware for the TM251MESE PLC using SoMachine V4.3?

Product Line:
M251

Resolution:
The latest M251 firmware is 4.0.6.37, which can be found in the Controller Assistant after you install SoMachine V4.3
Was this helpful?
What can we do to improve the information ?