Product FAQs

Ask a Question

Can you open the enclosure door of a Enclosed drive while its running?

Issue:
Can you open the enclosure door of a Enclosed drive while its running?

Product Line:
ATV660, E-flex, Econonflex, S-flex

Environment:
All 

Cause:
Door has interlock and can not be opened

Resolution:
The only way you can open the door on the enclosed drive is to turn off the disconnect first.  You can not and should not try and open the door of an enclosed drive when its running.
Was this helpful?
What can we do to improve the information ?