Product FAQs

Ask a Question

Are ATV6** and ATV9** integrated in SoMachine 4.3?

SoMachine V4.3 integrates the state of the art Schneider Electric Altivar variable speed drives ATV6** and ATV9** families. It offers the new function blocks Control_ATV to control the full ATV control range.
These drives complete the ATV340/320 from a power range point
- ATV320 : 0,18kW -> 15kW
- ATV340 : 0,75kW -> 75kW
- ATV6**: 0,75kW -> 800kW
- ATV9**: 0,75kW -> 800kW

The Control_ATV Function Block allows you to perform:
- A simple start application - Velocity control - Use a visu for commissioning independently from the fieldbus (CANopen, Modbus TCP, EtherNet/IP) and for (almost) all the Altivar family in order to help migration and machine update for more flexibility and scalability.
Was this helpful?
What can we do to improve the information ?