Product FAQs

Ask a Question

What to consider when adding a background image for an HMI in Vijeo Designer?

When adding a background image on an HMI, here are a few things to consider:

1) Ensure the image resolution of is the same as the HMI's screen resolution. This will save DRAM. If you simply add a large resolution image (ie.18 MegaPixel), it will consume too much DRAM on the HMI.
2) The file types supported are PNG, JPG, and BMP.
3) Put the background image on a Master Panel for easy re-use throughout your project.
Was this helpful?
What can we do to improve the information ?