Product FAQs

Ask a Question

What can cause an INFE fault on the ATV320 drives?

Issue:
What can cause an INFE fault on the ATV320 drives?

Product Line:
ATV320 drive

Environment:
All 

Cause:
CPU Error 

Resolution:
inFE is an internal CPU error.
Try power cycling the drive and if it does not reset you will need to replace the drive. 
Check the Drives firmware to see if its V2.7IE32 or above.
Was this helpful?
What can we do to improve the information ?