Product FAQs

Ask a Question

Is there a pulse input feature in our variable speed drives ranges to measure the speed of rotation of the motor?

On ATV32, a possibility is to connect a "Pulse input" to measure the speed of rotation of the motor.
Here below the attached pages & configuration parameters
Was this helpful?
What can we do to improve the information ?