Product FAQs

Ask a Question

What position does the SW103 switch need to be in to activate the termination resistor for bacnet on the ATV212 drives?

Issue:
What position does the SW103 switch need to be in to activate the termination resistor for bacnet on the ATV212 drives?

Product Line:
ATV212

Environment:
All 

Cause:
Position of the dip switch to active the terminator resistor. 

Resolution:
To active the terminator resistor put the switch position to the left.  See the dot on top of the switch in the example file this is ON. 
Was this helpful?
What can we do to improve the information ?