Product FAQs

Ask a Question

Video: How do I access Bits in a Word with SoMachine 4.1?

Memory words are 2 Bytes. To access the Bytes, double the address. For example, %MW100 is equal to %MX200.0..7 and %MX201.0..7.

The following video demonstrates this procedure:

 
Was this helpful?
What can we do to improve the information ?