Product FAQs

Ask a Question

Is there a replacement for the Twidoport module 499TWD01100?

There is no replacement for the Twidoport module 499TWD01100.

- 499TWD01100 is part of the Twido line of controllers which at this point is obsolete. It was used primarily to add an Ethernet port to a Twido controller without one.
- The replacement for the Twido controllers are the M221 controllers. All M221 controllers have an Ethernet port, this is the reason there is no replacement for this 499TWD01100.
- A customer looking for a 499TWD01100 should be looking into converting his Twido project to a M221 / SoMachine Basic project. A Twidosuite project can be opened and converted easily into a SoMachine Basic project.
- Please contact the automation technical support at 888-266-8705 if you need to convert a Twido controller to a M221 controller.
Was this helpful?
What can we do to improve the information ?