Product FAQs

Ask a Question

Is there a replacement for the TWDXCPMFK32 memory cartridge?

There is no replacement for the TWDXCPMFK32 memory cartridge.

- TWDXCPMFK32 is part of the Twido line of controllers which at this point is obsolete.
- The replacement for the Twido controllers are the M221 controllers. All M221 controllers have a SD card that can be used to transfer or backup a program.
- A customer looking for a
TWDXCPMFK32 should be looking into converting his Twido project to a M221 / SoMachine Basic project. A Twidosuite project can be opened and converted easily into a SoMachine Basic project.
- Please contact the automation technical support at 888-266-8705 if you need to convert a Twido controller to a M221 controller.
Was this helpful?
What can we do to improve the information ?