Product FAQs

Ask a Question

What are the SoMachine / CoDeSys Compiler Version Mappings?

The following mapping table gives an overview of which CoDeSys compiler version is used by default in a certain SoMachine version.
 
SoMachine Software Version
Mapped Display Version
CoDeSys Compiler Version
SoMachine V1.0
V1.0.10.0
3.2.2.43
SoMachine V1.1
V1.1.10.0
3.3.1.2
SoMachine V2.0 RL1
V2.0.18.8
3.3.1.40
SoMachine V2.0 RL2
V2.0.20.20
3.3.1.40
SoMachine V3.0
V3.0.14.5
3.4.1.50
SoMachine V3.1
V3.1.10.1
3.4.1.90
SoMachine V4.0
V4.0.0.0
3.5.3.60
SoMachine V4.1
V4.1.0.0
3.5.3.82
SoMachine V4.1 SP1
V4.1.0.1
3.5.3.83
SoMachine V4.1 SP1.1
V4.1.0.2
3.5.3.84
SoMachine V4.1 SP1.2
V4.1.0.3
3.5.3.85
SoMachine V4.1 SP2
V4.1.0.4
3.5.3.86
SoMachine V4.2
V4.1.0.4
3.5.3.86
SoMachine V4.3
V4.1.0.5
3.5.3.87
 
The mapped display version is used for example in the Project Settings → Compile Options dialog and the Project Update dialog.
Was this helpful?
What can we do to improve the information ?