Product FAQs

Ask a Question

Which Ethernet services does the M221 controller supports with SoMachine Basic V1.6?

The M221 logic controller supports the following services with SoMachine basic V1.6:
Modbus TCP Server
Modbus TCP Client
EtherNet/IP Adapter
Modbus TCP Slave Device
Was this helpful?
What can we do to improve the information ?