Product FAQs

Ask a Question

Can you advice sampling rate for Micom P14x & Micom P54x relays?

For a P14x, the relay uses 24 samples per cycle, this is 1200Hz sampling frequency (50Hz), 1440Hz sampling frequency (60Hz). 
For a P54x, the relay uses 48 samples per cycle, 2400Hz sampling frequency (50Hz) or 2880Hz sampling frequency (60Hz).
 
Was this helpful?
What can we do to improve the information ?