Product FAQs

Ask a Question

I would like to find out If the occupancy sensors and switches you have can accommodate lights and air conditioners

The attached data sheet will confirm the difference between the two sensors.

SAE-UE-MS-CU-WE

Load 1 :
 
  • Incandescent Lamp => Max.2000W
  • AC Halogen Lamp => Max.1000W
  • LV Halogen Lamp => Max. 1000VA
  • Fluorescent Lamp Max => 900VA/100μF
  • Energy Saving Lamp (includes CFL and PL lamp) => Max. 80VA
 
 
Load 2 :
 
  • HVAC => Max. 10A for ≤ 250VAC, p.f. = 1 Max. 5A for ≤30VDC

CCT551012 sensor only provides the following :
  • Load type :Halogen lamp with standard electronic transformer : 1200 VA
  • LED lighting : : 400 W
  • Motor : : 100 W
  • Halogen lamp with standard ferromagnetic transformer : 1200 VA
  • Fluorescent tube : 1200 VA, 140 µF
  • Compact fluorescent lamp : : 400 W
  • Relay : : 5 A - 250 V
  • Halogen lamp : : 1200 W - 230 V
  • Incandescent lamps : : 2300 W - 230 V
 
 
Was this helpful?
What can we do to improve the information ?