Product FAQs

Ask a Question

What is the technical difference between LC1D80008 & LP1D80008?


- Both reference get the same technical performance. 
- Both reference are screw clam terminals- Operational voltage is the same. 

The only difference coming from the past is 
- LC1D80008 is only AC coils reference 
- LP1D80008 is only DC coils reference. 

Looking in our commercial data base you will see that all reference starting with LC1D are only AC coils reference, while LP1D is only DC coils reference. 

You will never find LC1D80008 with DC coils
Was this helpful?
What can we do to improve the information ?