Product FAQs

Ask a Question

What is the burden of MES114(SEPAM relay I/O module)

Please find the below example to calculation the burden for MES114

If the input supply voltage is 125VDC then
 
Burden for one MES114 =125x3mA(available in the manual_the same is attached)=0.375 VA
 
Was this helpful?
What can we do to improve the information ?