Product FAQs

Ask a Question

What are the protocols available in Micom P40 relays

 Micom P40 relays will support Modbus* or IEC60870-5-103 or PRP(Parallel Redundancy Protocol) or HSR (High-availability Seamless Redundancy ) or
 RSTP(Rapid Spanning Tree Protocol )or Self Healing Ring(SHR) or DNP 3.0(Distributed Network Protocol)

*Few relays will not have this protocol .Please check with our local sales or marketing team before finalize the relay type
 

Need to order the relay with correct hardware or order number to support for any of the above protocol

 
Was this helpful?
What can we do to improve the information ?