Product FAQs

Ask a Question

Connect to the LMC078 by USB cable

Issue:
Connect to the LMC078 by USB cable

Product Line:
LMC078

Resolution:
To connect to the LMC078 motion controller using a USB cable, you have to manually set the COM port that was assigned to the cable in the SoMachine gateway, before scanning to find the controller in SoMachine (see attached)
Was this helpful?
What can we do to improve the information ?