Product FAQs

Ask a Question

Video: How to setup a 4-20mA loss fall back function on an ATV212 drive?

Issue:
Configuring 4-20mA Loss Fall Back Function on Altivar 212

Product Line:
Altivar 212

Environment:
All models.

Cause:
Setup

Resolution:
To program this function:
  1. Press Mode and arrow down to F--- and enter.
  2. Go to F644 and F649. F644 defines the action taken when a loss of 4-20mA is detected.
  3. F649 only applies if the F644 parameter is programmed to fall back to a speed (2).  


 
Was this helpful?
What can we do to improve the information ?