Product FAQs

Ask a Question

In Schneider Electric's global offer, do you offer ATEX enclosures suitable for Zone0, Zone 1 and Zone 2?

The Schneider Electric offer is designed to be used in group II and is classified as category 2 (Zone 1). So yes, we do have in our offer Zone 1 ATEX enclosures and this implies using them in a less harsh environment (Zone 2) but we do not offer enclosures for Zone 0. Customer could select the dimensions and the enclosure material that would suit his application from the attached document.

For more understanding on the ATEX topic, please refer to the highlighted text in the file attached to this case (Extract - UE15MK03EN.pdf) 
Was this helpful?
What can we do to improve the information ?