Product FAQs

Ask a Question

How can I extract the bytes from a located word variables in SoMachine V4.3

This can be done by creating 2 new byte variables with the address assignment as shown below:

B1 AT %MB0: BYTE; 
B12AT %MB1: BYTE; 
W1 AT %MW0: WORD

%MW0 uses %MB0 + %MB1.  %MB and %MW share the memory allocation in the SoMachine controller.
Was this helpful?
What can we do to improve the information ?