Product FAQs

Ask a Question

What is the sampling rate for CM4000T?


For CM4000T, in normal mode, it will record up to 512 samples per cycle, which is 25600Hz or 30720Hz depending on the system frequency; 

However, during a high-speed event, (transient events which last less than one cycle), the CM4000T will sample at 5Mhz or 83,333 samples per cycle (based on a 60Hz system). 
Was this helpful?
What can we do to improve the information ?