Product FAQs

Ask a Question

How to send smart notification like Mail directly from PME 8?

The latest version of the software, PME8.x, includes an EMAIL module in VIP (A new ION module), which can manage authentication.  The module can be used to create smart notifications, to learn more about, here some useful links with videos and TVD (It requires some engineering). This officially has addressed the requests about email authentication.

1, ION reference with new modules
https://exchangecommunity.schneider-electric.com/message/61243#61243

2. Video about EMAIL module
https://exchangecommunity.schneider-electric.com/docs/DOC-10305

3[PME8] [TVD] How Can I Use Smart Notifications to Detect Changes That Could Impact My Facility? (A TVD that uses the email module)
https://exchangecommunity.schneider-electric.com/thread/20185

In addition, other way to tackle the issue is to use Event Notification Module, *Which require additional license*. Here an overview: https://exchangecommunity.schneider-electric.com/thread/18705

 
Was this helpful?
What can we do to improve the information ?