Product FAQs

Ask a Question

How to reset Trio radio like J series to factory default incase IP address or other settings are unknown ?

If the radio settings become unknown then a factory reset is required. A factory default can be initiated by applying DC power to the radio (wait 45 seconds), depress the factory default switch using a paper clip or similar object and keep the switch depressed for 5 seconds until all five LEDs illuminate solid GREEN indicating the radio will return to the factory default settings.
Please wait 30 seconds for the factory default reset process to complete. Later you may use default IP address 192.168.2.15 to connect and configure. A factory reset will cause all previous configuration settings to be erased and returned to the factory default values.
Was this helpful?
What can we do to improve the information ?