Product FAQs

Ask a Question

Getting error E6111 on LXM32 drive

Issue:
Getting error E6111 on LXM32 drive

Product Line:
LXM32

Resolution:
Error 6111 appears when you try to perform a second movement (commands from the field bus) at the same time that auto-tuning is being performed.
To avoid this, you must deactivate access from the bus (stopping the master for example) during the auto-tuning operation.
Was this helpful?
What can we do to improve the information ?