{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What is the accuracy class of iEM2155 meter ?

Following are the Accuracy Class Details:

Active energy : class 1 according to IEC 62053-21
Active energy : class B according to EN 50470-3
Reactive energy : class 2 according to IEC 62053-23

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.